Dispose of a task

Dispose of a task

You can dispose of a task at runtime. You cannot run a task that you disposed of.

Stop()
method

Each asynchronous task automatically ends when the NetLogic parent node is removed. Nevertheless, we recommend disposing of tasks inside the
Stop()
method by invoking the
Dispose()
method, as shown in the following example.
public override void Stop() { myTask.Dispose(); }
IMPORTANT: Invoking the
Dispose()
method on an asynchronous task blocks it until the code ran by the task returns the control to the caller (through control of the task state or for completion of the task).

Example

The following example shows creating, running, and disposing of an asynchronous task.
public override void Start() { myTask = new PeriodicTask(IncrementVariable, 1000, LogicObject) myTask.Start(); } public override void Stop() { myTask.Dispose(); } private void IncrementVariable() { variable1.Value = variable1.Value + 1; } private PeriodicTask myTask;
The example involves:
  • Defining a private instance variable (
    private PeriodicTask myTask;
    ) in the C# class contained in the NetLogic.
    TIP: Depending on the type of task to be created, the class of this variable must be
    PeriodicTask
    ,
    DelayedTask
    , or
    LongRunningTask
  • Defining a method (
    IncrementVariable()
    ) that the task must run.
  • Creating the task.
    Inside the
    Start()
    method, in the C# class contained in the NetLogic, the private instance variable (
    myTask
    ) is initialized using the class constructor (
    PeriodicTask
    ).
    TIP: The constructor requires a variety of arguments based on the class to which it belongs. See Asynchronous task.
  • Executing the task as soon as the NetLogic is initialized at runtime.
    Inside the
    Start()
    method in the C# class contained in the NetLogic, the
    Start()
    method is invoked on the task (
    myTask.Start()
    ).
  • Disposing of the task in the
    Stop()
    method by invoking the
    Dispose()
    method.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.