Configure the debugger

Configure the debugger

Configure the Visual Studio or Visual Studio Code debugger.
  1. From the main toolbar, select
    Open .NET Solution
    .
    The default external code editor opens.
    TIP: We recommend using Microsoft Visual Studio 2022 or Microsoft Visual Studio Code as the default code editor. Some development assistance features may not be available when using a different code editor.
  2. If you use Visual Studio:
    1. From the
      Debug
      menu, select
      Attach to Process
      .
      A window that shows all processes running on the machine appears.
    2. Next to
      Attach to
      , choose
      Select
      and select
      Automatic
      . Select
      OK
      .
    3. In
      Available Process
      , select either:
      FTOptixRuntime.exe
      Debugs a runtime NetLogic.
      FTOptixStudio.exe
      Debugs a design-time NetLogic.
    4. Select
      Attach
      .
      The debug mode starts.
  3. If you use Visual Studio Code:
    1. Open the
      Run and Debug
      pane by pressing
      Ctrl
      Shift
      D
      .
    2. From the list at the top of the pane, select either:
      Attach to FTOptixRuntime (NetSolution)
      Debugs a runtime NetLogic.
      Attach to FTOptixStudio (NetSolution)
      Debugs a design-time NetLogic.
    3. Select
      Start Debugging
      or press
      F5
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.