Edit the code after debugging
The initialization of the debugging process is different for design-time and runtime NetLogics.
- Select an option:
- If you are debugging a NetLogic at runtime, fromFactoryTalk Optix Studiotoolbar, select.Stop
- If you are debugging a NetLogic at design time, in Visual Studio or Visual Studio Code, selectto stop debugging.
- Edit the code and save the editedCSfiles.FactoryTalk Optix Studioautomatically recompiles the .NET solution.
Provide Feedback