Alarm controller

Alarm controller

BrowseName
AlarmController
SuperType
Object(BaseObjectType)

Properties

Name
BrowseName
DataType
Description
Enabled
Enabled
Enable/disable the alarm.
Active
Active
Active/inactive alarm.
Auto acknowledge
AutoAcknowledge
True: when the alarm activates, it is automatically acknowledged and confirmed. False: when the alarm activates, it must be acknowledged by the user.
Auto confirm
AutoConfirm
True: when the alarm activates, it is automatically confirmed by the application. False: when the alarm activates, it must be confirmed by the user.
Input variable
InputValue
Variable to monitor.
Message
Message
Alarm message text.
Severity
Severity
Level of severity of the alarm, which indicates its priority on a scale from 1 to 1000 (in compliance with the OPC UA standard: 1 = information, 1000 = serious error).
Last event
LastEvent
Last alarm event generated.

Methods

Acknowledge
BrowseName
Acknowledge
InputArguments
Name
DataType
Description
EventId
EventID that identifies a particular event notification.
Comment
Localized text to apply to the alarm.
Confirm
BrowseName
Confirm
InputArguments
Name
DataType
Description
EventId
EventID that identifies a particular event notification.
Comment
Localized text to apply to the alarm.
Add comment
BrowseName
AddComment
InputArguments
Name
DataType
Description
EventId
EventID that identifies a particular event notification.
Comment
Localized text to apply to the alarm.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal