Data grid column
Data grid object column.
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Title | Title | Panel title, to be displayed in the navigation tab of a Navigation panel object. If not set, the panel BrowseName is displayed. | |
Width | Width | Width of column. Auto resizes columns when the Data grid is resized. Numeric value maintains specified column size when the Data grid is resized. | |
Header alignment | HeaderAlignment | Horizontal alignment of the content in the header row. | |
Content alignment | ContentAlignment | Horizontal alignment of the content in the rows other than the header row. | |
Order by | OrderBy | Attribute/property of the nodes or column of a table by which to sort the elements. Generally the same attribute/property or column from which the elements are obtained is set. | |
Data item template | DataItemTemplate | Data item template object which can contain data in textual or image format. |
Provide Feedback