Accordion example
Use this object to expand or collapse content blocks at runtime.
Accordion example
![](/content/dam/dita/en/factorytalk-optix/1-03/_images/accordion.png/_jcr_content/renditions/original)
Use case
Show or collapse blocks of secondary content in a panel.
TIP:
To add content to the
Accordion
object, insert graphical elements to the Header
and Content
objects.Provide Feedback