Checkbox example
Use this object to set and view a Boolean value at runtime.
- Selected checkbox
- The associated variable value is True.
- Cleared checkbox
- The associated variable value is False.
Checkbox example
![animated graphic showing selecting and clearing a Checkbox](/content/dam/dita/en/factorytalk-optix/1-03/_images/ref_checkbox_ex.png/_jcr_content/renditions/original)
Use case
Enable or disable functions or features within a
FactoryTalk Optix Application
. For example, toggle a graph that visualizes data.Provide Feedback