LED example
Use this object to display a Boolean value as an LED that is on or off.
LED
objects can contain text or an image.LED example
![Animated graphic showing a red LED light being either on or off](/content/dam/dita/en/factorytalk-optix/1-03/_images/ref_led_ex.png/_jcr_content/renditions/original)
Use case
Signal an alarm status, a mechanical component function, or a software function.
Provide Feedback