Configure a Navigation panel

Configure a Navigation panel

Configure a
Navigation panel
by referencing Panel objects as tabs.
  1. In
    Project view
    , create or select a
    Navigation panel
    object.
  2. Create
    Panel
    types that you want to reference as tabs in the
    Navigation panel
    .
  3. Select
    Navigation panel
    . In
    Properties
    add tabs by selecting
    Add
    next to
    Panels
    .
  4. Create dynamic links between
    Panel
    properties and
    Panel
    types.
    For more information about dynamic links, see Create dynamic links.
  5. (optional) Change tab titles by editing the
    Title
    property values.
  6. (optional) Add images to tabs by editing the
    Image path
    property values.
    TIP: The image overrides the panel Title or BrowseName. For seamless integration with the UI, use correctly sized flat images with a transparent background.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal