- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
OPC UA server example
Use this object to publish project nodes to the OPC UA client project.
Use case
Publish the selected project nodes to the selected users through the OPC UA client.
TIP:
The OPC UA server publishes all child nodes and all parent nodes of the selected nodes. Multiple clients can connect to a single-server endpoint.
Provide Feedback