Vertical layout example
Use this object to lay out the interface elements in the X-axis evenly.
Horizontal layout example
The positioning and distance between the buttons depend on the margins set on these buttons.
![](/content/dam/dita/en/factorytalk-optix/1-03/_images/ref_ColumnLayout_ex02.png/_jcr_content/renditions/original)
Use case
Lay out interface elements vertically. For example, lay out buttons or other objects.
TIP:
To achieve a different order of the interface elements, arrange the objects in the model.
Provide Feedback