Configure FactoryTalk Optix display engine

Configure FactoryTalk Optix display engine

Configure an Ubuntu client system to display
FactoryTalk Optix Applications
with the
FactoryTalk Optix Studio
display engine.
TIP: You can display
FactoryTalk Optix Applications
in a web browser instead of using the
FactoryTalk Optix Studio
display engine. Displaying applications in a web browser does not require additional display engine configuration on client systems. For more information, see Presentation Engines.
  1. Verify that the X11 windows manager is installed.
    TIP: Ubuntu Desktop installations include the X11 windows manager by default.
  2. Disable the Wayland manager by uncommenting
    #WaylandEnable=false
    in
    /etc/gdm3/custom.conf
    .
  3. In terminal, enter
    sudo apt install -y libxcb-xinerama0
    to install the Xinerama extension of X11.
  4. Enter
    sudo apt install -y libevent-dev
    to install a dependency that manages alarms.
  5. (optional) Enter
    sudo apt install -y gstreamer1.0-libav ubuntu-restricted-extras
    to install dependencies that render videos at runtime.
    TIP: Depending on the video codec used, you may need to install more dependencies.
  6. Restart the system.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal