Install FactoryTalk Optix Application Update Service

Install FactoryTalk Optix Application Update Service

Install
FactoryTalk Optix Application Update Service
on an Ubuntu client system.
  1. Download the most recent version of
    FactoryTalk Optix Application Update Service
    installer script from
    FactoryTalk Hub
    .
  2. In the terminal, navigate to the download directory.
  3. Enter
    sudo chmod +x ./
    installer_script
    .sh
    to make the script executable.
  4. Enter
    sudo ./
    installer_script
    .sh
    to run the installer script.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal