Set options
Specific global settings for the
FactoryTalk Optix Studio
software. Global settings include the language displayed on the user interface, activation of the log messages, activation of features under development, the default code editor for any NetLogic C# code, the unit of measurement for physical lengths, and version control settings.
- In theFactoryTalk Optix Studiotitle bar, select the drop-down arrow afterand selectFactoryTalk Optix Studio OptionsFactoryTalk Optix Studio Options.
- InFactoryTalk Optix Studio Options, complete:
- Language. Select the language for the user interface.
- Advanced mode. Activate the advanced log messages displayed in theOutputpane.
- Show feature previews. ActivateFactoryTalk Optix Studiofeatures that are under development and may create instability in projects.
- Preferred code editor. Set the default code editor for any NetLogic C# code
- Preferred physical length unit. Set the default unit of measurement for physical lengths.
- UnderVersion Control User Configuration, complete:
- User Name. The username of the logged in user account when a project is stored in a version control repository.
- User Email. The email address of the logged in user account when a project is stored in a version control repository.
- UnderVersion control providers and IDs, inSelect a provider, select the username authorized to store projects in the version control repository and then selectAdd identity.
- SelectSave.
Provide Feedback