Configure a widget to display logged alarms
Add a widget that displays historical data about alarms at runtime.
- From the toolbar, select.Template Libraries
- InLibraries, search forAlarm History Grid with filter.
- UnderComponents, dragAlarm History Grid with filterontoPage3 (type)inProject view.
- SelectClose.
- InProject view, selectFilteredAlarmHistoryGrid1.
- InProperties, setHorizontal alignmenttoStretch.The object adjusts its width to the container at runtime.
- Create a dynamic link betweenAlarmsEventLoggerand .For more information about dynamic links, see Create dynamic links.
Filtered Alarms History Grid with filter in Page3

Provide Feedback