Associate the LED status with the switch
Turn the LED object on and off with the switch.
- InProject view, selectLED1.
- InProperties, create a dynamic link betweenActiveand .For more information about dynamic links, see Create dynamic links.
LED toggle
![](/content/dam/dita/en/factorytalk-optix/1-03/_images/quick-start-led-off.png/_jcr_content/renditions/original)
![](/content/dam/dita/en/factorytalk-optix/1-03/_images/quick-start-led-on.png)
Provide Feedback