Configure a recipe
Create a recipe schema that uses the Ingredient01, Ingredient02, and Ingredient03 variables.
- From theFactoryTalk Optix Studiotoolbar, select.Open dashboard page
- In the central pane, selectI want to configure a recipe.
- SelectNew recipe.
- Create a dynamic link betweenTarget nodeand:
- If you created variables,.
- If you imported Logix controller variables,.
- SelectNextand selectNext.
- SelectNew database.
- InName, enterRecipeDBand selectNext.
- SelectNextand selectNext.
- SelectIngredient01,Ingredient02, andIngredient03, and selectNext.Selected variables
- SelectExit.
In 
Project view
, RecipeSchema1
appears under Recipes
.
Recipe schema object

Provide Feedback