FactoryTalk Optix Studio web version
You can use
FactoryTalk Optix Studio
in a web browser through FactoryTalk Hub
.Editor features support
FactoryTalk Optix Studio web version
supports all FactoryTalk Optix Studio desktop version
features except for:
- Save logs from theOutputtabs.
- Edit NetLogic files.
- OpenFactoryTalk Optix StudioHelp Center.
- Display paths in logs in theOutputtabs.
- Draw lines, polylines, rectangles, and ellipses in the editor.
- Add and use custom fonts.
- Add files and images by dragging and dropping them intoFactoryTalk Optix Studio web version.
- Restart the application at runtime by using themethod.
Emulator features support
FactoryTalk Optix Studio web version
emulator supports all features of FactoryTalk Optix Studio desktop version
emulator except for:
- Display animations in the runtime emulator.
- Control theWebBrowserobject in the runtime emulator.
- Control thePDFViewerobject in the runtime emulator.
- Control theVideoobject in the runtime emulator.
- Control theWindowobject in the runtime emulator.
Provide Feedback