Communication drivers overview
Some Communication drivers may have specific characteristics.
Communication driver | Online tags import | Offline tags import |
---|---|---|
Modbus Driver | ![]() | |
MELSEC FX3U Driver | ![]() | |
S7TCP driver | ![]() | ![]() |
OMRON EtherNet_IP driver | ![]() | |
MALSEC Q driver | ![]() | |
S7 TIA PROFINET driver | ![]() | ![]() |
OMRON Fins Driver | ![]() | |
ASEM EtherNet_IP Driver | ![]() | ![]() |
CODESYS Driver | ![]() | ![]() |
TwinCAT driver | ![]() | ![]() |
Serial port | ![]() | |
RA EtherNet_IP Driver | ![]() | ![]() |
Provide Feedback