Organize the imported tags

You can organize the imported tags into folders. The tags imported into
FactoryTalk Optix Studio
remain synchronized with the controller after moving them into different folders.
IMPORTANT: We do
not
recommend separating and reorganizing the tags contained in a structured tag since their initial structure is restored if the tag is synchronized again.
  1. In the
    Project view
    pane, locate the
    Tags
    object associated with a
    Communication station
    .
  2. To create a folder, right-click the
    Tags
    object and select
    New
    Folder
    .
  3. Move the imported tags into the folder.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.