Key-value converter
Convert the value of the source to its corresponding parent value based on a table of key-value pairs. The key-value converter converts heterogeneous data, such as a color to value.
ValueMap editor
You can open the ValueMap editor by selecting
next to the key-value converter in Advanced Dynamic Link Editor.
![Edit](/content/dam/dita/en/factorytalk-optix/1-03/_images/editorpropertiesblack.png/_jcr_content/renditions/original)
The the ValueMap editor includes:
![](/content/dam/dita/en/factorytalk-optix/1-03/_images/KeyValueConverter.png/_jcr_content/renditions/original)
Item | Description |
---|---|
A | Converter toolbar. Select ![]() Delete |
B | Data type selector. |
C | Key-value table. |
Properties
Property | Description |
---|---|
Mode | The direction of the dynamic link:
|
Source
A variable with a value corresponding to a key.
TIP:
The first row defines the default value if no corresponding key is found. In the example, if the Key value is 10 and no corresponding line is found, the output value Monday is returned.
Output
The value associated with the key in the map.
Logical representation
Example of a logical conversion in the
Complex Dynamic Link Editor:
TIP:
Select
to open the ValueMap editor if necessary.
![Edit](/content/dam/dita/en/factorytalk-optix/1-03/_images/editorpropertiesblack.png/_jcr_content/renditions/original)
![](/content/dam/dita/en/factorytalk-optix/1-03/_images/converter_key_value_representation.png/_jcr_content/renditions/original)
Provide Feedback