- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Create a dynamic link by dragging the source
Create a dynamic link by dragging the source from
Project view
to the value of the property that you want the dynamic link to set. - InProject view, select the variable that contains the property that you want to set through the dynamic link.
- Drag the node or variable to either a:
- Property. Drag the node to the value of the property.The reference to the node or variable appears in the property.
- Graphic object. Drag the variable to a graphic object in the editor.This creates a dynamic link to the most suitable property of the graphical object. For example, drag a variable to aTextBoxto create a link to theTextproperty and display the value.
The reference to the selected node or variable appears in the property. For more information, see References to dynamic link sources.
Provide Feedback