Create a dynamic link by selecting the source
Create a dynamic link using the
Properties
pane.- InProject view, select the node that contains the property to set through a dynamic link.
- InPropertiesnext to the property value to set, select.Add Dynamic Link
- In theDynamic Linksbrowser, select a node to act as the source of the value property.
- (optional) To select a node attribute as the source, inAttribute, select an attribute.For example, selectBrowseName,Value, orDisplayName.
- (optional) If you select an array variable as the source, inArray Index, enter the index value of the variable to use.
- ChooseSelect.
The reference to the selected node or variable appears in the property. For more information, see References to dynamic link sources.
Provide Feedback