- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Parent node format
If a dynamic link is set between two nodes of the same data type, you can set the format for the parent node.
Data types of the source node used to set the parent node format include:
Source node data type | Parent node format | Description | Example |
---|---|---|---|
| 0 (1234) | Binary representation, without the thousands separator | 7.989 ► 7989 |
Hexadecimal (ff) | Hexadecimal representation | 45 ► 2d | |
Octal | Octal representation | 80 ► 55 | |
Binary | Binary representation | 45 ► 10010110 | |
FloatDouble | 0,# (1234,5) | Rounding to the first decimal place |
|
0,## (1234,56) | Rounding to the second decimal place |
| |
0,### (1234,56) | Rounding to three decimal places |
| |
0.0 (1234.0) | Representation with exactly one decimal place |
| |
0.00 (1234.00) | Representation with exactly two decimal places |
| |
0.000 (1234.000) | Representation with exactly three decimal places |
| |
DateTime | hh:mm | Date/time format, t | 05:30 |
dd/MM/yy | Date/Time format, d | 01/05/19 | |
hh:mm:ss | Extended date time format, T | 06:01:58 | |
d MMM yyyy | Extended date, format D | 1 gen 2019 | |
dd/MM/yy, hh:mm | Extended date/time, format g | 01/07/2016, 12:59 | |
d MMM yyyy, hh:mm:ss | General date/time layout, format F | 1 feb 2019, 6:15:28 | |
yyyy-MM-ddThh:mm:ss.0000000Z | ISO 8601 Standard, format o or O | 2019-01-07T00:00:00.0000000Z | |
Duration | [d.]hh:mm:ss[.0000000] | Format c | 2.09:10:2006:10:20 |
[d:]h:mm:ss[,0000000] | General short format, g | 4:9:10:20 | |
d:hh:mm:ss,0000000 | General extended format, G | 4:09:20:15,0000000 |
Provide Feedback