Apply animations to graphic objects
Add and configure number, sequential, or parallel animation properties to animate a graphic object.
- InProject view, select the graphic object to animate.
- InProperties, at the top, selectand then select either:
- Number animation.
- Sequential animation.
- Parallel animation.
For more information, see Animations. - Configure animation properties. See Animation properties.
Provide Feedback