Align graphic objects
Align selected items vertically or horizontally in the Design Area. Aligning objects increases and decreases the margins of the selected items.
- InProject view, double-click a container or select. The User Interface Editor opens.
- In the editor, select the graphic objects to align. To select multiple objects, hold downCtrland select additional items.
- In the Design Area toolbar, select the icon to align the selected graphic objects in the Design Area:
Align at the left border.
Aligns at the top border.
Align at the right border.
Align at the bottom border.
Provide Feedback