Change the order of graphic objects

Change the order of graphic objects

Move selected graphic objects in front of or behind other graphic objects in the Design Area.
  1. In
    Project
    , double-click a container or select
    Editor
    .
  2. In the Design Area of the User Interface Editor, select the object to move.
    TIP: To select multiple graphic objects, hold down
    Shift
    and select additional objects.
  3. In the Design Area toolbar, select the button to move the graphic object in relation to the other graphic objects:
    • Send to back
      . Send the graphic object behind all objects in the Design Area.
    • Send backward
      . Send the graphic object behind the next object in the Design Area.  
    • Bring forward
      . Send the graphic object in front of the next object in the Design Area.
    • Bring to front
      . Send the graphic object in front of all objects in the Design Area. 
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal