Configure a style sheet
Configure a style sheet to change the properties of the style sheet. Some style properties display a preview in the editor.
- InProject view, expand theUIfolder and double-click the style sheet.The style sheet andPropertiesopen.
- InProperties, configure the properties of the style sheet:TIP: To change a property value, selectto enter a value manually, or selectto browse for and link to a tag that has the value to display.Add Dynamic Link
- Name. Select the current name to edit the name of the style sheet. Type a new name and pressEnter.
- Type. This property isStyle sheetby default and is read-only.
- Window color. Select the background color of the window.
- Border width. Select the default width of graphic object borders. Enter the value manually or selectto link to a tag with the value you want to display.Change Dynamic Link
- Text color. Select the color of text graphic objects.
- Border color. Select the color of graphic object borders.
- Focus color. Select the color of a graphic object that is in focus at runtime.TIP: Select the box that represents the color and then inSelect Color, drag to select the color and chooseSelect.
Provide Feedback