Import fonts
You can configure your
FactoryTalk Optix Application
to use custom fonts in TTF
or OTF
format. To use a font other than a default, import the font into the project to make it available as a graphic object property.
TIP:
Instead of performing this procedure, you can copy custom folder.
TTF
or OTF
font files into the ProjectName
\ProjectFiles\Font- In the main toolbar, select.Browse project files
- InProject Files, select.Import file(s)
- Navigate to and select the font to import and then selectOpen.
- CloseProject Files.
The font is now available in the
Font family
properties of graphic objects.Provide Feedback