Use an existing style sheet
Use a style sheet included in
FactoryTalk Optix Studio
. You can also create and configure a custom style sheet.- Select.Template Libraries
- InLibraries, selectStyleSheetsto open the style sheets in the project.
- Drag the desired style sheet into theUIfolder ofProject view.
Graphic objects located under the folder that contains the style sheet in
Project view
now inherit the styles configured in the style sheet.Provide Feedback