Configure the grid in the User Interface Editor
Configure the grid in the User Interface Editor to show or hide the grid, align objects in the grid, and size the grid.
- InProject view, double-click a window or container object, or select. The User Interface Editor opens.
- In the editor toolbar, select.
- Select the option to configure the grid:
- Grid Visible. Toggle showing the grid in the editor.
- Snap to grid. Align the edges of objects with the grid.
- Grid size. Specify the size of the grid in pixels.
Provide Feedback