Resize the window

Resize the window

Set the size of the window object to specify the size of the Design Area.
  1. In
    Project view
    , select the window object.
  2. In
    Properties
    , in
    Height
    , enter the value for the height of the window.
  3. In
    Width
    , enter the value for the width of the window.
  4. (optional) In
    Full Screen
    , select
    True
    to make the user interface the same size of as the screen at runtime.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.