- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Azure IoT Hub broker
Push Agent for Azure IoT Hub supports only the secured communication mode.
The secured communication mode involves the client authentication through an SAS Token generated for each device that wants to send or receive messages from Azure IoT Hub.
The client authenticates with username and password, for example:
- username
- contoso.azure-devices.net/MyDevice01/?api-version=2018-06-30
- password
- SharedAccessSignature sig=signature-string&se=expiry&sr=URL-encoded-resourceURI
Provide Feedback