Create a remote library
Create a custom remote library to store templates of objects and variables.
- From the main toolbar, select.Template Libraries
- InTemplate Libraries, selectand selectNew remote library.
- InRemote location, enter a URL to a Git repository to store the library.IMPORTANT: Verify that the Git repository is safe to store the remote library. Contact a repository administrator to learn who can access the repository.
- (optional) Enter a name for the library.
New local library appears in
Template Libraries
.Add templates to your library. See Create a template from an object or variable.
Provide Feedback