Push a library
Push changes to the remote library to the remote Git repository.
- From the main toolbar, select.Template Libraries
- SelectPush.
The library is backed up to the remote Git repository.
Provide Feedback