Data logger

Data logger

A data logger samples the values of one or more variables at user-defined intervals or at every value change and stores them in a database.
TIP: You can disable automatic sampling by setting the
Sampling mode
property to
None
.

Database configuration

FactoryTalk Optix Studio
automatically configures databases for data loggers.
When selecting a database for a data logger, for each variable to sample,
FactoryTalk Optix Studio
automatically creates and configures a database table with the following columns:
Column
Description
Present
[VariableToLogName]
The value of a specific variable
Always
[VariableToLogName]
_OpCode
The variable code of the reading operation on the controller
If
Log operation code of the variable = True
[VariableToLogName]
_Timestamp
The date and time (UTC) of the variable reading on the controller
If
Log timestamp of the variable = True
Timestamp
The date and time of the sample reading on the controller.
This timestamp refers to the time when
FactoryTalk Optix Studio
stops reading all sample variables.
Always
LocalTimestamp
The date and time of the variable reading on the controller in the machine local time zone.
If
Local time log = True

Automatic sample modes

A data logger can automatically sample:
All monitored variables
The data logger samples all monitored variables regardless of their values.
Only the variables with significantly changed values
Change in value
sampling mode applies only to the variables with significantly changed values.
The data logger samples only the variables which values vary beyond a deadband interval in comparison with the previous sampling. The deadband interval value can be an absolute or percentage value.
For example, if the deadband interval is set to
5
, the data logger samples only the variables that have an absolute or percentage variation of at least ±5 in comparison with the previous sampling.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal