Edit a data logger
You can edit data logger properties by using a wizard built into
FactoryTalk Optix Studio
.- From theFactoryTalk Optix Studiotoolbar, select.Open dashboard page
- In the central pane, selectI want to configure a data logger.
- Select the data logger that you want to edit.
- On the right, if needed, edit the logger name and properties.
- SelectNext.
- Select an existing database or configure a new database:
- To use an existing database:
- Select an existing database.
- If needed, edit the database properties.
- SelectNext.
- To create a database:
- SelectNew database.
- If needed, edit theNameandTypefields.
- SelectNext.
- If needed, edit the database properties.
- SelectNext.
- To duplicate an available database:TIP: Duplicating an existing database allows you to create a database base on the existing database quickly.
- Right-click an available database and selectDuplicate.
- If needed, edit the database properties.
- SelectNext.
- Select the variables to log.TIP: You can find the variables to select quickly using theSearchfield.
- SelectNext.
- Review the settings.
- SelectExit.
Provide Feedback