Export translated strings to a CSV file
Export strings to use in the strings another project and help prevent having to recreate and translate the strings. Export translated strings to a CSV file using the predefined script in the template library.
- In the main toolbar, select.Template Libraries
- SelectScripts.
- UnderComponents, dragTranslations Importer and Exporterinto the project node orTranslationsfolder.
- InTemplate Libraries, selectClose.
- WithImport and Export Translationsselected, inProperties, inCSVPath,browse to select the .CSV file.
- InCharacterSeperator, select the separator.
- InProject view,right-clickImport and Export Translationsand then selectExecute ExportTranslations.
Provide Feedback