- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Use translated texts in a string formatter
Create a reference to a translation key to have the key use the related translated text according to the session locale at runtime. A translation key is a reference to a specific translation in the translation dictionary.
- InFormatproperty, type characters present in the key. The keys containing the typed characters appear.
- Select a key and then pressEnter.
If the text for the key contains placeholders for the string formatter sources, such as “{0}”), the relative properties appear.
Provide Feedback