Display content in Project view
To display the content of interest in
Project view
, collapse nodes to see only the higher structure of the project or split Project view
to see different areas of the information model simultaneously.- In theProject viewtoolbar, select either:
- Navigate backward. Select the previously selected node or item.
- Navigate forward. Select the most recently selected node or item.
- (optional) Collapse all nodes for easier navigation. Right-click the root project node and then selectCollapse all.
- (optional) DivideProject viewinto two areas that you can scroll separately. SelectSplit project viewto divide the view. SelectSplit project viewagain to remove the division in the view.
- (optional) Search for content inProject viewinstead of having to navigate. InType to searchat the top ofProject view, type the name of the item. To clear search, select.
Provide Feedback