- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Open an object
Open an object from
Project view
. - InProject view, double-click the object or mouse over the object and then select.
The object opens if the object has a dedicated editor.
Properties
for the object open.Provide Feedback