Paths

You can use path shortcuts when developing your application logic.
Path shortcuts
Shortcut
Description
%PROJECTDIR%
A directory that contains files transferred at runtime (images, documents, and so on).
Example:
C:\Users\
UserName
\Documents\Rockwell Automation\FactoryTalk Optix
\
ProjectName
%APPLICATIONDIR%
A directory that contains objects used at runtime, including these objects:
  • Embedded Database
  • Retentivity Storage
  • Exported files
%USB
N
%
,
where
N
is a number associated with the USB device.
A path to a specific USB device connected to the target device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.