- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
View references of a node or item
View references to display all of the objects in the information model that reference a node or object.
- View references fromProject view.
- InProject view, right-click the node or item and then selectShow References.
- InReferences of (name), select a location and then selectGo to ...
FactoryTalk Optix Studio
navigates to the location of the reference. Objects referenced in a NetLogic are not shown.Provide Feedback