Import an OPC UA NodeSet

Import an OPC UA NodeSet

Import an OPC UA NodeSet in either online or offline mode.
Prerequisites
  1. To import an OPC UA NodeSet
  2. In
    Project view
    , right-click the OPC UA client object and select
    New
    OPC UA tag importer
    .
    OPCUATagImporter
    appears under the OPC UA client object.
  3. Next to
    OPCUATagImporter
    , select
    Editor
    .
  4. Configure the NodeSet import:
    • If you import the NodeSet in the online mode, set the toggle to
      Online
      .
    • If you import tags in the offline mode:
      1. Set the toggle to
        Offline
        .
      2. In
        File path
        , provide a path to the
        XML
        file with the NodeSet.
  5. Select the items to import and then select
    Apply
    .
The imported objects appear under the OPC UA client.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal