Import nodes at design time
Import nodes by using the OPC UA tag Importer object.
Prerequisites
- InProject view, right-click an OPC UA client object and select .
- Double-click theOPCUATagImporterobject.
- FactoryTalk Optix Studioconnects to the server.
- In the central pane, the editor shows the list of nodes that can be imported.
- AnObjectsnode is created inside theOPCUAClientobject.
- In the editor, select the nodes and selectSynchronize.
The project nodes corresponding to the selected nodes are added to the
Objects
node.Provide Feedback