Configure firewall for an OPC UA server
If an application has an OPC UA server running in Windows®, open the port specified in the
Endpoint URL Server
property of the OPC UA server.Prerequisites
- When running a project with an OPC UA server object, if prompted, accept requests for configuring a firewall rule.
The
firewall rule is created.runtime
Provide Feedback