- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Backup a project
FactoryTalk Optix Studio
automatically creates backups of projects. Projects are automatically backed up:
- When you save a project
- When you update a project to make the project compatible with a more recent version ofFactoryTalk Optix Studio
- Every time you update a project to repair a corrupted project. See Restore a project.
The default location for the backup folder is:
%localappdata%\Rockwell Automation\FactoryTalk Optix\Studio\Backups\
Project Name
Each of the project folders consists of other subfolders with these different types of backups:
- Automatic. Three backups, performed when saving the project.
- Recovery. One backup, performed when a corrupt project is opened and repair attempted inFactoryTalk Optix Studio. See Restore a project.
- Upgrade. Two backups, performed when updating the project to make it compatible with a newer version ofFactoryTalk Optix Studio.
Provide Feedback