- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Reuse objects from the default recipes editor
You can use the objects from the default recipes editor widget as building blocks of a custom recipe management solution.
- InProject view, right-clickRecipesand select .
- Select theRecipesEditorobject and select.LockThe graphical objects associated with theRecipesEditorobject display.
- Develop a custom management recipes interface.For more information, see Custom recipes management interface.
- Remove the defaultRecipesEditorwidget that you created in 1.
Provide Feedback