Duplicate a recipe schema

Duplicate a recipe schema

Duplicate a recipe schema based on the existing recipe schema.
  1. From the
    FactoryTalk Optix Studio
    toolbar, select
    Open dashboard page
    .
  2. In the central pane, select
    I want to configure a recipe
    .
  3. Right-click the available recipe schema and select
    Duplicate
    .
If necessary, edit the duplicated recipe schema. See Edit a recipe schema.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.