Sessions and locales
A session is a runtime context in which a user executes read and/or write operations based on their permissions.
The session displays information, such as the groups to which the user belongs and their locale. This information can be used to create dynamic interfaces based on the permissions of the user, settings, or custom property of the user.
Provide Feedback